AXIS#.SAFEPARAM.SBT.MAXTIMEINTERVAL

Description

Indicates the time in minutes that Safe Brake Test (SBT) must be executed before a warning becomes active that indicates SBT should be run and the Safe Brake Acknowledge (SBA) signal becomes low.

If the SBT period has elapsed the drive will permit enabling and movement. It is up to the safety system design to prevent motion, if required.

 

Parameters Editor with the Maximum Time Interval row circled

Context

For complete SBT information refer to SBT (Safe Brake Test).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

02-01-02-000

General Information

Type

Read/Write

Units

Minutes

Range

1 – 480 minutes

Default Value

480 minutes

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SBT.MAXTIMEINTERVAL

3157h

02h

Unsigned32

-

-

Read/Write

No

AXIS2.SAFEPARAM.SBT.MAXTIMEINTERVAL

3257h

02h

Unsigned32

-

-

Read/Write

No